The thermal protection behavior can be
split up into three categories of events that can happen. Thermal
Behavior shows each of these categories.
- Relative thermal shutdown:
the device is enabled into an overcurrent event. The output current rises up to
the IILIM level and the FLT goes low. With this
large amount of current going through the junction temperature of the FET
increases rapidly with respect to the controller temperature. When the power FET
temperature rises TREL amount above the controller junction
temperature ΔT = TFET – TCON > TREL, the
device shuts down. For auto-retry version, after tRETRY, the part
tries to restart itself. Latch version will require EN to be toggled to
re-enable the channel. The FLT is asserted until the fault
condition is cleared. The first plot in Thermal
Behavior shows the relative thermal shutdown behavior for the auto-retry version.
- Absolute thermal shutdown:
the device is still enabled in an overcurrent event. However, in this case the
junction temperature rises up and hits an absolute reference temperature,
TABS, and then shuts down. For auto-retry version, the device
does not recover until both TJ < TABS – Thys
and the tRETRY timer has expired. For latch version, toggling EN is
required to re-enable the channel. The second plot in Thermal
Behavior shows the absolute thermal shutdown behavior for the auto-retry version.
- Latch version: the device
is enabled into an overcurrent event. The DIAG_EN pin is high so that
diagnostics can be monitored on SNS and FLT. For the latched version of the
device, if the part shuts down due to a thermal fault, either relative thermal
shutdown or absolute thermal shutdown, the device does not enable the channel
until the EN pin is toggled. The third plot in Thermal
Behavior shows the relative thermal shutdown behavior for the latch version.