SLVSHM2A March 2025 – August 2025 TPS2HC120-Q1
PRODUCTION DATA
This device has several states to transition into based on the ENx pins, DIAG_EN pin and load conditions.
In the SLEEP state, everything inside the device is turned off and the quiescent current is the ISLEEP. The device can only transition out of the SLEEP state if the ENx pins or DIAG_EN pin gets pulled high. From SLEEP, the device can transfer into the ACTIVE state if any of the ENx pins are pulled high, or the DIAGNOSTIC state if the DIAG_EN pin, without any of the ENx pins, goes high. Additionally, if the device is in any of the states and VBB drops below VUVLOF, the device transitions into SLEEP state.
The DIAGNOSTIC state is when the device is outputting diagnostics on the SNS and FLT pins. This can happen when the device is in any previous state and the DIAG_EN pin goes high. The off-state diagnostics are comprised of open load detection in off state and short to battery detection. The FLT pin asserts if there is a fault on any of the channels, but the SNS pin only outputs a fault for the channel associated to the SELx pin values. From the DIAGNOSTIC state, the device can transfer into the ACTIVE state if the DIAG_EN pin goes back low and any channel is on or the STANDBY DELAY state if all channels are OFF.
The ACTIVE state is when any of the channel outputs are on by the ENx pin associated. In the ACTIVE state, the current limit value is set by the external resistor on the ILIM pin. If the DIAG_EN pin is pulled high while in the ACTIVE state, the SNS pin outputs a proportional current to the load current of the channel associated to the SELx pins configuration until a fault occurs on that channel. Additionally the FLT pin reports if there is a fault occurring on any channel. The device can transition out of the ACTIVE state by turning off all of the channels while DIAG_EN is high or low, or a fault occurring. If all of the channels turn off and DIAG_EN is high, the device transitions into the DIAGNOSTIC state. If all of the channels turn off and the DIAG_EN pin is low, then the device transfers into the STANDBY DELAY state.
The STANDBY DELAY state is when the ENx pins are all low, outputs are all turned off and the DIAG_EN pin is also low but there has not yet been tSTBY amount of time. This state is included so that the channel outputs can be PWM'd without all of the internal rails being cut off and put to SLEEP mode. Once the device has waited tSTBY, the device completely shuts down and transitions into SLEEP. However, if during tSTBY, ENx were to go high, the device transitions into ACTIVE without shutting completely down. Similarly if the DIAG_EN goes high, the device transitions into DIAGNOSTIC.
The LOW POWER MODE state is when the channels that are active are below the ILPM,entry level for longer than tSTBY and the DIAG_EN is low. The device turns off all unnecessary internal blocks and reduces the quiescent current from IQ to IQ,LPM. The device is still protected but no diagnostics or fault reporting is possible until device comes out of this mode. For more information on Low Power Mode see Low Power Mode.