SLVSI46 July 2025 DRV8818A
ADVANCE INFORMATION
During PWM current chopping, the H-bridge is enabled to drive through the motor winding until the PWM current chopping threshold is reached. This is shown in Figure 6-2, Item 1. The current flow direction shown indicates positive current flow in the step table below.
Once the chopping current threshold is reached, the H-bridge can operate in Fast Decay, Slow Decay, or Smart Tune Dynamic Decay mode. The decay mode setting is latched at power-up or when exiting sleep mode.
| DECAY | RCA | Decay Mode |
|---|---|---|
| 0 | 12kΩ to 100kΩ | Fast Decay |
| 1 | 12kΩ to 100kΩ | Slow Decay |
| 0.21 × VCC < VDECAY < 0.6 × VCC | 12kΩ to 100kΩ | Mixed Decay |
| X | GND | Smart Tune Dynamic Decay |
In fast decay mode, once the PWM chopping current level has been reached, the H-bridge reverses state to allow the winding current to flow in a reverse direction. If synchronous rectification is enabled (SRn pin logic low), the opposite FETs are turned on; as the winding current approaches zero, the bridge is disabled to prevent any reverse current flow. If SRn is high, current is recirculated through the body diodes or external Schottky diodes. Fast-decay mode is shown in Figure 6-2, Item 3.
In slow-decay mode, the winding current is re-circulated by enabling both of the low-side FETs in the bridge. This is shown in Figure 6-2, Item 2.
If SRn is high, current is recirculated only through the body diodes, or through external Schottky diodes. In this case, fast decay is always used.
The DRV8818A also supports a mixed decay mode. Mixed decay mode begins as fast decay, but after a while switches to slow decay mode for the remainder of the fixed off time.
Fast and mixed decay modes are only active if the current through the winding is decreasing; if the current is increasing, then slow decay is always used.
Which decay mode is used is selected by the voltage on the DECAY pin. If the voltage is greater than 0.6 × VCC, slow decay mode is always used. If DECAY is less than 0.21 × VCC, the device operates in fast decay mode when the current through the winding is decreasing. If the voltage is between these levels, mixed decay mode is enabled.
In mixed decay mode, the voltage on the DECAY pin sets the point in the cycle that the change to slow decay mode occurs. This time can be approximated by:

Mixed decay mode is only used while the current through the winding is decreasing; slow decay is used while the current is increasing.
Operation of the blanking, fixed off time, and mixed decay mode is illustrated in Figure 6-3.
Figure 6-3 PWMThe smart tune dynamic decay current regulation scheme is an advanced current-regulation control method compared to traditional fixed off-time current regulation schemes. Smart tune current regulation helps the stepper motor driver adjust the decay scheme based on factors such as:
Figure 6-4 Smart tune Dynamic Decay ModeSmart tune Dynamic Decay greatly simplifies the decay mode selection by automatically configuring the decay mode between slow, mixed, and fast decay. This eliminates the need for motor decay tuning by automatically determining the best mixed decay setting that results in the lowest ripple and best performance for the motor. Smart Tune Dynamic Decay is best for applications that require minimal current ripple, at the same time maintain a fixed frequency with the current regulation scheme.
Select Smart Tune Dynamic Decay mode by connecting the RCA pin to GND.
After the current is enabled (start of drive phase) in an H-bridge, the current sense comparator is ignored for some time (tBLANK) before enabling the current-sense circuitry. The blanking time also sets the minimum drive time of the PWM. The blanking time is approximately 1.25µs.
The decay mode setting is optimized iteratively each PWM cycle. If the motor current overshoots the target trip level, then the decay mode becomes more aggressive (increases fast decay percentage) on the next cycle to prevent regulation loss. If a long drive time must occur to reach the target trip level, the decay mode becomes less aggressive (decreases fast decay percentage) on the next cycle to operate with less ripple more efficiently. With decreasing current steps, smart tune Dynamic Decay automatically switches to fast decay to reach the next current step quickly.
The off time tOFF during Smart Tune Dynamic Decay mode can be selected by setting the RCB pin to Hi-Z or ground as shown in Table 6-2.
| RCA | RCB | OFF Time |
|---|---|---|
| GND | Hi-Z (Floating) | 16µs |
| GND | GND | 32µs |