SLVSIM9 September 2025 LM5125A-Q1
PRODUCTION DATA
Monitor the average VI input current at the IMON-pin. The average sensed current of each active phase is summed up generating a source current at the IMON-pin, which is converted to a voltage by the resistor RIMON. The resulting voltage VIMON is calculated according to Equation 18, the required resistor RIMON according to Equation 17. VIMON regulates up to 3V and is self-protecting not reaching the absolute maximum value.
RCS1 and RCS2 are the respective phase sense resistors. For a disabled phase use 0Ω as sense resistor value, add additional sense resistor values for each active phase in dual device configuration. IIN is the input current, GIMON the transconductance gain, n the number of active phases and IOFFSET the offset current given in the electrical characteristics table.
Limit the average input current by choosing an appropriate resistor connected to the ILIM-pin. When the input current limit is active, VOUT is regulated down until the set average input current limit is reached. In case VOUT is regulated below the VI voltage the current is unlimited. The DLY-pin capacitor CDLY adds an additional delay time tDLY to activate and deactivate the average input current limit (see Figure 6-23). When the ILIM-pin voltage reaches the threshold VILIM (typical 1V) the source current IDLY is activated charging up the DLY-pin capacitor CDLY. The DLY-pin voltage VDLY rises until VDLY_peak_rise is reached, which activates the average input current limit. The ILIM-pin voltage is regulated to VILIM and the input current is regulated down to the average input current limit set by RILIM resulting in a VOUT drop. To exit the average current limit regulation the output load has to decrease, which causes VOUT to rise and VILIM to fall below VILIM_reset (typical 0.88V). VILIM_reset activates the sink current IDLY, which discharges the DLY-pin capacitor CDLY. When VDLY reaches VDLY_peak_fall the average input current limit is deactivated and the DLY-pin is discharged to VDLY_valley. The required resistor RILIM is calculated according to Equation 19.