SLVSIM9 September 2025 LM5125A-Q1
PRODUCTION DATA
The open-loop response of a boost regulator is defined as the product of modulator transfer function and feedback transfer function. When plotted on a dB scale, the open loop gain is shown as the sum of modulator gain and feedback gain. The modulator transfer function of a current mode boost regulator includes a power stage transfer function with an embedded current loop. The transfer function is simplified as one pole, one zero, and one right-half-plane zero (RHPZ) system.
The modulator transfer function is defined as follows:
where
If the equivalent series resistance (ESR) of Cout (RESR) is small enough and the RHPZ frequency is far away from the target crossover frequency, the modulator transfer function is further simplified to a one pole system and the voltage loop is closed with only two loop compensation components, RCOMP and CCOMP, leaving a single pole response at the crossover frequency. A single pole response at the crossover frequency yields a very stable loop with 90 degrees of phase margin.
As shown in Figure 7-1, a gm amplifier is utilized as the output voltage error amplifier. The feedback transfer function includes the feedback resistor divider gain and loop compensation of the error amplifier. RCOMP, CCOMP, and CHF configure the error amplifier gain and phase characteristics, create a pole at origin, a low frequency zero and a high frequency pole.
Feedback transfer function is defined as follows:
where
The pole at the origin minimizes the output steady state error. Place the low frequency zero to cancel the load pole of the modulator. Use the high frequency pole to cancel the zero created by the output capacitor ESR or to decrease noise susceptibility of the error amplifier. By placing the low frequency zero an order of magnitude less than the crossover frequency, the maximum amount of phase boost is achieved at the crossover frequency. Place the high frequency pole beyond the crossover frequency because the addition of CHF adds a pole in the feedback transfer function.
The crossover frequency (open loop bandwidth) is usually limited to one fifth of the RHPZ frequency.
Increase RCOMP and proportionally decreasing CCOMP for higher crossover frequency. Conversely, decreasing RCOMP while proportionally increasing CCOMP, results in lower bandwidth while keeping the same zero frequency in the feedback transfer function.