SLVSJD0 September 2026 DRV8003-Q1
PRODUCTION DATA
Figure 9-2 DRV8003-Q1 Component Placement and LayoutThe layout screen shot above shows the device component and layout relative to the device. This layout screen shot comes from the device evaluation module. Note that all power supply decoupling capacitors, especially smaller values, and charge pump capacitors are placed as closed to the pins as possible and are placed on the same layer of the device. All general guidelines outlined in the previous section are followed in the evaluation module layout design when possible.