SLVSMQ4 September 2026 TPS7H5101-SEP
ADVANCE INFORMATION
D-CAP+ is a control architecture optimized for high-current, low duty cycle multiphase regulators. It utilizes adaptive on-time control. In this control method, rather than varying the duty cycle to maintain voltage regulation as is the standard with peak current mode control, the high-side FET is turned on for a predetermined amount of time once the control loop triggers the turn-on. However, in contrast to classic constant on-time control, in which the on-time is the same regardless of the operating conditions, adaptive on-time allows for variation based on the input voltage, output voltage, and load to maintain a pseudo-constant frequency during steady state operation.
The controller senses current from the converter using an output from the power stages or inductor sensing, whether using the inductor DCR or a series resistor. The current from each phase is sensed and summed internally to the controller to generate the ISUM signal. The on-time pulses are generated by the controller when the valley of the sensed current waveform ISUM intersects with the error correction signal VDROOP at the output of the droop amplifier. Note that the D-CAP+ method does not require an internal oscillator, but the SW_CLK signal corresponding to the intersection of ISUM and VDROOP is generated each time the on-time pulse is triggered on either phase.
In the case of multiphase operation, the phase manager is used to distribute the SW_CLK signal to the appropriate phase with the proper interleaving of 180°. During single phase operation, ISUM corresponds to the single phase current and SW_CLK generates a pulse on the same phase for each cycle. Figure 7-1 shows the basic waveforms for D-CAP+, in which VDROOP can be seen to contain a component of the output voltage ripple.