SLVSMQ4 September 2026 TPS7H5101-SEP
ADVANCE INFORMATION
When the voltage at the enable pin is below the enable rising threshold, the device is in shutdown mode and the controller does not produce any output pulses. The device is enabled by bringing the voltage at the pin above this threshold, and after being enabled, the device can be disabled by reducing the voltage below the enable falling threshold. There are several ways in which the device can be enabled externally. A resistor divider from VIN to GND can be used to supply the EN voltage.
The resistors can be appropriately sized to turn on the device at the desired input voltage, as shown in Equation 10. This implementation creates an adjustable UVLO that complements the default internal UVLO thresholds on VIN.
where
Likewise, Equation 11 can be used to calculate the VIN(falling) voltage.
where
Alternatively, the EN pin can be driven directly from a microcontroller or FPGA. The low voltage threshold of the enable pin supports logic levels as low as 1.1V.
As discussed in Section 7.5, the TPS7H5101 can also be enabled and disabled through the PMBus interface. As such, there can be a condition where EN is externally above the necessary threshold for turn-on, but the device remains disabled based on the commanded state via PMBus. The default state for the PMBus enable is “on”, and as such at startup when then the EN pin is driven high the device is enabled without any initial PMBus command.