SLVUBY7A October 2020 – October 2022 DRA821U , LP8764-Q1 , TPS6594-Q1
The TPS6594141B GPIO8 is configured as an input to disable the watchdog. Typically, during development this pin is tied high, so that when the nRSTOUT bit is set WD_PWRHOLD is also set. The configuration of this pin can be utilized for other features or functions but this requires servicing the watchdog before it expires. The watchdog long window is 772 seconds.
Write 0x12:0x09:0x00:0xBF // Disable Watchdog
Write 0x48:0x38:0x01:0x00 // configure GPIO8 as a pushpull output
When it is time to enable and configure the watchdog, then in addition to enabling the watchdog the WD_PWR_HOLD must be cleared.
Write 0x12:0x09:0x00:0xFB // Clear WD_PWRHOLD
Write 0x12:0x09:0x40:0xBF // Enable Watchdog