SLVUC05A November 2020 – July 2022 TPS25750
Description | The 'PBMe' Task ends the patch loading sequence. This Task instructs the PD controller to complete the patch loading process. |
---|---|
INPUT DATAX | . |
OUTPUT DATAX | Byte 1: Standard Task Return Code. See also Table 3-1. |
Task Completion | The 'PBMe' Task completes after it has ended the patch loading sequence. If MODE register (0x03) is equal to 'APP ', then this Task will be rejected. |
Side Effects | When the 'PBMe' is successful, the second slave address will be restored to the value configured by the ADCINx pins. The PD controller leaves the MODE register (0x03) as 'PTCH' and will wait for the patching process to restart. |
Additional Information | If the MODE register is 'APP ' indicating that the PD controller is in the APP mode, then it will reject the 'PBMe' Task. |