SLVUCP8A September 2024 – June 2025 TPS26750
To generate a new configuration for the TPS26750EVM, click the Reset Configuration button on the top right side of the tool (this is next to the Flash To Device drop-down menu). This button erases the existing configuration and resets the form back to the default settings. TI recommends to export the existing form before resetting, so that the existing configuration is not lost. For details on how to save configurations, refer to Section 3.4.6.2.