Note: The red highlighting shows
active or
powered portions of the EVM for the specific setup in
Figure 2-1 and
subsequent block diagrams.
Required hardware setup:
- Ensure jumper J11 is connected.
- Connect USB-C end of USB-C to USB-C cable or USB-A to USB-C cable to Data Type C port (J6).
- Connect other end of cable to computer.
When flashing a new configuration to the TPS26750EVM, the binary configuration file is written to U13, the EEPROM. More details are provided in
Section 3.4.6.3.