SLVUD37 December 2024
The TPS62968EVM was used to take all the data in the TPS62968 data sheet. See the device data sheet for the performance of this EVM.
The thermal performance of the EVM is shown in the following figure.
Figure 3-1 Thermal Performance (VIN = 12V, VOUT = 0.6V, IOUT = 8A, JP2 700kHz)