WARNING:  |
| The TPS62968EVM circuit module can become hot during
operation due to dissipation of heat. Avoid contact with the
board. Follow all applicable safety procedures applicable to
your laboratory. |
CAUTION:  |
| Do not leave the EVM powered when unattended. |
WARNING: The circuit module has signal traces,
components, and component leads on the bottom of the board. This can result in
exposed voltages, hot surfaces, or sharp edges. Do not reach under the board during
operation.
CAUTION: The circuit module can be damaged by over
temperature. To avoid damage, monitor the temperature during evaluation and provide
cooling, as needed, for the system environment.
CAUTION: Some power supplies can be damaged by
application of external voltages. If using more than one power supply, then check
the equipment requirements and use blocking diodes or other isolation techniques, as
needed, to prevent damage to the equipment.
CAUTION: The communication interface is not isolated
on the EVM. Be sure no ground potential exists between the computer and the EVM.
Also be aware that the computer is referenced to the battery-potential of the
EVM.