SLVUD44A March 2025 – October 2025 TPS1689
Use the following instructions to perform the output hot short test:
The test waveforms of output hot short on the TPS1689EVM are shown in Figure 3-9 and Figure 3-9.
Figure 3-8 Output Hot Short Response (Zoomed Out) in TPS1689EVM (VIN = 54V, RIMON = 1.24kΩ, RIREF = 40.2kΩ, RSFT = 150kΩ, and COUT = 1mF)To obtain repeatable and similar short-circuit testing results is very difficult. The following contributes to the variation in results:
The actual short exhibits a certain degree of randomness because the short microscopically bounces and arcs. Make sure that configuration and methods are used to obtain realistic results. Hence, do not expect to see waveforms exactly like the waveforms in this user's guide because every setup is different.