SLVUDD5 July   2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents (Required Equipment)
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 Setup Procedure
      1. 2.1.1  Installing the DAC39RF20EVM Configuration GUI Software
        1. 2.1.1.1 Installing and Setting Up Vivado™ Lab Tools
      2. 2.1.2  Connect the DAC39RF20EVM and TSW14J59EVM
      3. 2.1.3  Connect the Power Supplies to the Boards (Power Off)
      4. 2.1.4  Connect the Spectrum Analyzer to the EVM
      5. 2.1.5  Turn On the TSW14J59EVM Power and Connect to the PC
      6. 2.1.6  Turn On the DAC39RF20EVM Power Supplies and Connect to the PC
      7. 2.1.7  Turn On the Signal Generators
      8. 2.1.8  Launching the DAC39RF20EVM GUI and Programming the DAC EVM - JMODE 0 (Bypass Mode)
      9. 2.1.9  Launching the DAC39RF20EVM GUI and Programming the DAC EVM - JMODE 1 (DUC Mode)
      10. 2.1.10 Configuration Example of DAC39RF20EVM in DDS Mode
    2. 2.2 Evaluation Board Details: Analog Outputs
    3. 2.3 FMC Signal Routing
  7. 3Hardware Design Files
  8. 4Additional Information
    1. 4.1 Trademarks

Connect the Power Supplies to the Boards (Power Off)

  1. Confirm the power switch on the TSW14J59EVM is in off position. Connect the power cable to a 12V DC (minimum 5A) power supply. Make sure the proper supply polarity by confirming the outer surface of the barrel connector is GND and the inner portion of the connector is 12V. Connect the power cable to the TSW14J59EVM power connector.
  2. DAC39RF20EVM can be powered with 12V DC (minimum 3A) though the connector jack (J2) on the DAC39RF20EVM, or the EVM can be powered from the TSW14J59EVM by FMC+ connector. There is a switch (SW1) which can be used to select power from the barrel jack on the DAC EVM, or from TSW14J59EVM through FMC+ connector. Confirm that the power switch for the DAC39RF20EVM power supply is set to the opposite position (jack) from where the the EVM is drawing power. If using barrel jack option, then connect the power cable to a 12V DC (minimum 3A) power supply. Make sure the proper supply polarity by confirming that the outer surface of the barrel connector is GND and the inner portion of the connector is 12V. Connect the power cable to the EVM power connector. Table 2-1 is used as a reference to power the DAC39RF12EVM.
Table 2-1 Powering the DAC39RF12EVM
DAC39RF20 Powered FromDAC39RF20 Power Switch PositionTSW14J59EVM FMC Switch PositionPower Supply Needed
TSW14J59EVM by FMC+ connectorFMCON12V 5A for TSW14J59EVM
External supply with jack on DAC39RF20EVMJACKOFF12V 3A for TSW14J59 and 12V 3A for DAC39RF20EVM
CAUTION: Make sure the power connections to the EVMs are the correct polarity. Failure to do so can result in immediate damage. Leave the power switches in the off position until directed later.