Use the following guidelines to set up the equipment:
- Set power supply #1 (PS#1) for 20V ±100mVDC, with the current limit set
to > 5A. Turn off supply.
- Connect PS#1 output in series with a current meter (multimeter) to J2
(VIN, GND)
- Connect a voltage meter across J2 (VIN, GND)
- Connect a voltage meter across J3 (BAT, GND)
- Connect a voltage meter across J1 (SYS, GND)
- Make sure the jumpers are installed as
indicated in IO and Jumper Descriptions.
- For SMBus Communication, use the
following steps:
- Connect J6 to the EV2400. Connect J5
to theSMB PORT 1 on the EV2400
- Turn on the computer and PS#1. Open
the bqStudio software.
- Select Charger and click the
Next button.
- Select
Charger_1_00_BQ24810.bqz on the Select a Target Page.
- And then click the Registers
button.
- After selecting the target device,
click the Read Register button.
- Set WATCHDOG to disabled.