SLVUDF2 August 2026
After downloading the appropriate software, launch the GUI locally from the PC application or from the TI Cloud using the Gallery. To use the TI Cloud version of the GUI, click anywhere in the panel, shown in Figure 3-4, that is not associated with the download or information icons.
Figure 3-4 GUI Panel Within the
GalleryFigure 3-5 shows an example of the PC application.
Figure 3-5 PMIC GUI Desktop
Application