SLVUDF2 August 2026
First, take a look at the USB2ANY Interface Adapter User's Guide to make sure that the USB2ANY adapter has the proper firmware and components. Additional information on the adapter pin functions is included in the document.
To connect the EVM to a computer using the USB2ANY adapter, plug the ribbon cable from the USB2ANY into the J2 header on the EVM. The ribbon cable is keyed at both ends to make sure that all the pins are connected correctly. Plug the USB cable extending from the other side of the USB2ANY into a computer.