SLVUDF2 August 2026
Use the TPS65214-GUI in the browser or as a stand-alone application. This software provides a simple way to communicate with the device through I2C using the built-in USB2ANY using an MSP432. This section include details on the GUI installation and setup process. Note that the EVM can power up and operate without use of software.
This section describes the usage and capabilities of the TPS65214 Graphical User Interface (GUI) tool from Texas Instruments.