SLVUDG9 September 2025
With the EVM properly connected and software installed, launch the Single Wire Memory EVM GUI application. The software launches with a screen similar to that shown in Figure 2-2.
The GUI has two main sections: Memory Table, which enables manipulation of the main memory space on the device, and Status Registers, used to modify memory settings. Controls is always available, and is for controlling device communication.
The message shown in Figure 2-4 appears when the GUI is launched and the EVM was not detected. Check the USB connection and that the board appears in Device Manager.
Figure 2-4 Device Communication Error