SLVUDG9 September 2025
In the center of the GUI window, users see the Memory Table that displays the data stored in the memory. Each row represents individual memory pages on the device, while columns represent bytes in each page. Scrolling is necessary to view the entire table.
| Error | Explanation |
|---|---|
| Invalid character at row X and column Y | A cell in the table is edited to contain no value or an invalid byte. Cell is automatically filled with 0xFF values. |
| The data at row X and column Y has been padded. | A cell contains a valid byte, but is only 1 character. The upper nibble is padded with 0x0. |
| Data in table is not valid hexadecimal | Select Read from Memory again. |