SLVUDG9 September 2025
Selecting Read from Memory automatically populates that main device memory into the table. Allow a few moments for the read to occur. A Read memory success! message appears in the Status Console on a successful read.
| Error | Explanation |
|---|---|
| Please select a device | Device was not selected. Press Search Devices again and select a new device. |
| No Single-Wire devices detected | No Single-Wire devices were detected on the bus. Check the USB connection and the presence of the board in device manager. Make sure jumper J4 is installed in a position that powers the SDQ bus (TMF00XXEVM Test Points and Switches). |
| Target device is not present. Search again or select another device | The target device is not present on the bus. Check the physical connection of the memory device. |
Please note that in a situation where there are multiple devices on the bus and the user removes the target device from the bus, a Read Memory command populates the data table with values of FF and still receives a success message. This is because a presence pulse is pulled low from another device, but no device on the bus responds to the match ROM or subsequent read memory command. Due to the communication behavior as open-drain of Single-Wire, no response is interpreted as a 1 on the bus.