The UCC35131-Q1 integrated isolated power
design simplifies system design and reduces board area usage. Follow these guidelines for
proper PCB layout to achieve optimum performance. A minimum of 4-layer PCB layer stack using
2-ounce copper on external layers is recommended to accomplish a good thermal PCB design.
The recommendation is to not route signal tracks or place components directly beneath the
UCC35131-Q1.
- Input capacitors between VIN pin and GNDP
pin:
- Place the 0.1μF high frequency bypass
capacitor (C3) as close as possible to pins 3, 4 (VIN) and pins 5–8 (GNDP) and on the
same side of the PCB as the IC. 0402 ceramic SMD or smaller is a desired size for
optimal placement. The self-resonant frequency in a range between 10MHz to 30MHz is
best to offer low impedance decoupling for the switching frequency noise of the
internal isolated convertor. Do not place any vias between the bypass capacitor and
the IC pins so as to force the high frequency current through the capacitor.
- Place the bulk VIN capacitor(s) (C2)
as close as possible and parallel to the 0.1μF high frequency bypass capacitor (C3)
and on the same side of the PCB as the IC as shown in Figure 3-8.
- /PG decoupling capacitor: The /PG
decoupling capacitor should be placed close to pin 2 (/PG) and on the same side of the PCB
as the UCC35131-Q1. Refer to C13 placement shown in Figure 3-8.
- Output capacitors between VDD pin and COM
pin:
- Place the 0.1μF high frequency bypass
capacitor (C5) as close as possible to pin 12 (VDD) and pins 10, 11 (COM) and on the
same side of the PCB as the IC. 0402 ceramic SMD or smaller is a desired size for
placement. The self-resonant frequency in a range between 10MHz to 30MHz is best to
offer low impedance decoupling for the switching frequency noise of the internal
isolated convertor. Do not place any vias between the bypass capacitor and the IC pins
so as to force the high frequency current through the capacitor.
- Place the bulk VDD-COM capacitor (C8)
as close as possible and parallel to the 0.1μF high frequency bypass capacitor (C5)
and on the same side of the PCB as the IC as shown in Figure 3-8.
- Output capacitors between VEE pin and COM
pin:
- Place the 2.2μF high frequency bypass
capacitor (C9) as close as possible to VEE and COM pins. The self-resonant frequency
in 3MHz to 4MHz is best to offer low impedance decoupling for the switching frequency
noise of the buck-boost converter with the 3.3uH inductor (L1) selection. Putting the
capacitor on the different side of PCB and using vias to connect is possible, to
reduce the switching loop between the capacitor and the internal low-side MOSFET of
the VEE buck-boost converter. In addition, putting the capacitor on different side
also simplifies the decoupling capacitor placement of VDD pin and COM pin. An example
of bottom side PCB placement of C9 and L1 is shown in Figure 3-12.
- Feedback:
- COMA must be isolated through all PCB
layers, from the COM plane. Use one via to make a direct connection to the low-side
resistor and filter capacitor from FBVDD pin, same as the low-side filter capacitor
from FBVEE pin.
- Place the RFBVDD feedback resistors
(R6 and R7) and the decoupling ceramic capacitor (C6) close to the IC.
- The top-side feedback resistor must
be placed next to the low-side resistor with a short, direct connection between both
resistors and single connection to FBVDD pin. The top connection to sense the
regulated rail (VDD-COM) must be routed and connected at the VDD bias capacitor remote
location near the gate driver pins for best accuracy and best transient response.
- The VEE feedback resistor (R5) must
be placed with the decoupling ceramic capacitor (C4) next to FBVEE (pin 15); while the
connection to sense the regulated rail (COM-VEE) must be routed and connected at the
COM bias capacitor remote location near the gate driver pins for best accuracy and
best transient response.
- When using the dual output mode, the
buck-boost inductor (L1) and a 2.2uF decoupling ceramic capacitor (C9) must be
populated. These can be place on the opposite side of the IC or on the same layer as
IC.
- A layout example is shown in Figure 3-9, where L2 (yellow) is routed on layer 2 and L3 (green) is routed on
layer 3.
- Thermal vias: The UCC35131-Q1 internal
transformer makes a direct connection to the lead frame. It is therefore critical to
provide adequate space and proper heatsinking designed into the PCB as outlined in the
steps below.
- TI recommends to connect the VIN,
GNDP, VDD, and COM pins to internal ground or power planes through multiple vias.
Alternatively, make the polygons connected to these pins as wide as possible.
- Use multiple thermal vias connecting
PCB top side GNDP copper to bottom side GNDP copper. If possible, the recommendation
to use 2-ounce copper on external top and bottom PCB layers.
- Use multiple thermal vias connecting
PCB top side VEE copper to bottom side VEE copper. If possible, the recommendation is
to use 2-ounce copper on external top and bottom PCB layers.
- Thermal vias connecting top and
bottom copper can also connect to internal copper layers for further improved heat
extraction.
- Thermal vias should be similar to
pattern shown below but apply as many as the copper area allows. TI recommends to use
thermal via with 30mil diameter, 12mil hole size.
- A layout example is shown in Figure 3-10. For cases where less copper area is available, use as many thermal
vias as the design permits, placed close to pins 5-8 (primary) and 9-11
(secondary).
- Creepage clearance: To maintain the full
creepage, clearance and voltage isolation ratings specified in the data sheet, avoid
routing signal traces or placing components directly under the UCC35131-Q1. Maintain the
clearance width highlighted in red, throughout the entire defined isolation barrier.
Keep-out clearance for basic isolation can be 50% less than the reinforced isolation
requirement (8.2mm). Using 8.2mm provides additional margin. A layout example is shown in
Figure 3-11.
- Gate driver output capacitors: CVDD_GD
(C11 and C12) and CVEE_GD (C10) are reference designators referred to in the UCC35131-Q1
Excel Calculator Tool. C11 and C12 are the capacitors between VDD-COM and C10 is the
capacitor between COM-VEE. C10-12 are capacitors required by the gate driver IC.
- CVDD_GD and CVEE_GD must be placed
next to the gate driver IC for best decoupling and gate driver switching
performance.
- For best voltage regulation, the
feedback trace from VEE (FBVEE) and VDD (FBVDD) must be as direct as possible so that
the voltage feedback is being sensed directly at the VDD and VEE capacitors near the
gate driver IC.