SNAA406B August 2024 – May 2025 LMK6C
IBIS SI simulations were ran in MentorGraphics' Hyperlynx tool. Altium board files were exported to a free-form SI schematic, modeling the effect of transmission lines and stubs for actual PCB trace routing and layer stackup. Figure 2-1 shows a simplified simulation example with a LVCMOS clock driver, transmission line model, and load capacitance. After extracting PCB layout to an SI model, a series of transmission line models are added to the circuit to represent trace interconnects, passive component pads, stubs, and other factors impacting the trace impedance. The Hyperlynx waveform viewer allows the user to change the clock oscillation frequency along with the time and vertical scaling, similarly to a traditional oscilloscope. The probe is placed at the load capacitor rather than the driver to simulate what a receiver can detect in a real system.
Figure 2-1 Hyperlynx SI Simulation
Setup