SNAA406B August   2024  – May 2025 LMK6C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction and Test Methodology
  5. 2Simulation Setup
  6. 3Routing Topologies and Simulation Results
    1. 3.1 Single-Line
    2. 3.2 Star Line
    3. 3.3 Split Line
    4. 3.4 Star Line vs. Split Line
  7. 4Lab Measurements
    1. 4.1 Lab Measurement Setup
    2. 4.2 Lab Measurement Results and Correlation to Simulation Data
  8. 5Trace Length Mismatch Between Loads
  9. 6Application Example: FPD-Link
  10. 7Summary
  11. 8References
  12. 9Revision History

Star Line

The star line configuration is an alternative design designed for when loads are not co-located on a board. This configuration starts out as a single output line from the driver, then splits off closer to the receiver side. Star line routing is similar to the single-line approach, but with receivers that are further than 1" apart.

Line resistors (Rt) are added to aid in impedance matching so the driver sees a continuous 50Ω impedance. Rt is calculated according to the formula in Equation 1.

Equation 1. R t = N - 1 N + 1 × Z 0

Where N is equal to the number of loads being driven and Z0 is equal to the characteristic impedance of the trace.

 Star Line Topology Figure 3-4 Star Line Topology
 Star Line Simulation
                    Results Figure 3-5 Star Line Simulation Results
Table 3-2 Star Line Rise/Fall Time
Number of Loads Trace Length - LS Rise Time (ns) Fall Time (ns)
2 2" 1.858 2.206
2 6" 2.839 3.980

For star line configurations, as this is similar to the single line configuration, with only 2" of split trace length we see the rise and fall times are increased with very slight rippling. As the trace length increases to 6", rippling worsens and rise/fall time further increase. While this signal can be adequate to some receivers, increasing the split line length further can result in unacceptable signal integrity.