SNVSCO2 November 2025 LM51261A-Q1
PRODUCTION DATA
The switching frequency of 100kHz to 2.2MHz is set by the RT resistor connected between the RT-pin and AGND. The RT resistor is selected between 14kΩ and 316kΩ according to Equation 4. If configured to use an external clock the device uses the RT-pin to set the internal oscillator and synchronizes the switching frequency within ±50% to an external clock applied at the SYNCIN-pin. The external clock must be within the SYNCIN frequency activity detection range fSYNC_DET and fSYNC_DET_min to be detected. The internal clock is synchronized at the rising edge of the external clock signal applied at the SYNCIN-pin. The Spread Spectrum setting is ignored when external clock synchronization is selected and clock dithering is disabled.
The device always starts with the internal clock and starts synchronizing to an applied external clock during the START and the ACTIVE state (see Functional State Diagram). The device synchronizes to the external clock as soon as the clock is applied and switches back to the internal clock in case the external clock stops.