Select compensation components for a stable
control loop using the procedure outlined as follows.
- Based on a specified loop gain crossover
frequency, fC, of 30kHz, use the following equation to calculate
RCOMP, assuming an effective output capacitance of 61µF. Select a standard
value for RCOMP of 18.2kΩ. VREF is VOUT/10 if
VSTEP is 10mV. VREF is VOUT/20 if VSTEP is
20mV.
Equation 38.
- To provide adequate phase boost at
crossover while also allowing a fast settling time during a load or line transient, select
CCOMP to place a zero at the higher of (1) one tenth of the crossover
frequency, or (2) the load pole. Select a standard value for CCOMP of 2.7nF.
Equation 39.
- Calculate CHF to create a pole
at the ESR zero and to attenuate high-frequency noise on the COMP pin. CBW is
the bandwidth-limiting capacitance of the error amplifier. A negative CHF can
be ignored in this design. However, in noisy environments, especially at high
VIN and high load currents, additional capacitance can help filter out the
noise.
Equation 40.
Note: Set a fast loop with high
RCOMP and low CCOMP values to improve the response when recovering
from operation in dropout.