Use Equation 28 to calculate the required buck inductance based on a 40% inductor ripple current at
nominal input voltages.
Equation 28.
Select a standard inductor value of 15µH. Use
Equation 29 to calculate the peak inductor currents at maximum steady-state input voltage.
Subharmonic oscillation occurs with a duty cycle greater than 50% for peak current-mode
control. For design simplification, the device has an internal slope compensation ramp
proportional to the switching frequency that is added to the current sense signal to damp
any tendency toward subharmonic oscillation.
Equation 29.
Based on Equation 6, use Equation 30 to cross-check the inductance to set a slope compensation close to the ideal one times
the inductor current downslope.