SPRACU5E June 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The ADC0 inputs are connected to the AM64x GPIO1 module when configured to operate as general-purpose inputs (GPI). The assignment of each ADC0 pin to the GPIO1 module is defined in the ADC0 Signal Description table found in the data sheet. The inputs are able to perform the same input function as any other GPIO1 input. Please read the GPIO sections in the processor-specific TRM to understand the capabilities of these inputs.
For more information, see the following FAQ: