SPRAD20 March 2022 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
In configuration, most of EDMA module shown in Figure 2-29 will be updated by user defined function during initialization of application. So, most contents can stay as the default.
Figure 2-29 A Summary of EDMA
ConfigurationThe key is the EDMA Channel Trigger Configuration in Figure 2-30. All trigger sources are listed in the Channel Trigger menu. As shown earlier, EPWM7 is configured as the trigger for EDMA to update DAC generating resolver excitation sine wave.
Figure 2-30 EDMA Channel Trigger
Configuration