SPRAD20 March 2022 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
For a control card in Figure 2-2, it offers both JTAG and UART ports in one USB port. Details on hardware connection can be found in AM263x Control Card User's Guide. It is necessary to create a target configuration file for the debug ports. A step-to-step guide is given in screen shots from Figure 2-3 to Figure 2-10. Briefly, a target configuration file is created and then configured with both JTAG and UART. The UART COM Port in Figure 2-10 should match PC Device Manager COM Port for JTAG probe Application/User UART. The Baud Rate in Figure 2-10 should be consistent with SoC UART Baud Rate configured in next step.
Figure 2-2 AM263x Control Card
Figure 2-3 Create New Target
Configuration File
Figure 2-4 Select JTAG Connection and
Device
Figure 2-5 Add UART Communication
Port
Figure 2-6 Open Advanced Target
Configuration
Figure 2-7 Add Component
Figure 2-8 Select CPU Properties
Figure 2-9 Find XDS110 UART COM
Port
Figure 2-10 Update CPU Properties in
Advanced Target Configuration