SPRAD67D September 2024 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Selection of the required processor OPN is an important phase during custom board design. To get an overview of the processor family architecture and for selecting the required processor OPN (that can be used in the custom board) based on the required functionality and features, package (ALV (AM64x, AM243x) and ALX (AM243x)) and speed grade, see the Functional Block Diagram, Device Comparison, Device Naming Convention, Device Speed Grades and Packaging Information sections of the device-specific data sheet.
See the Device Comparison chapter, Device and Documentation Support section of the device-specific data sheet to choose the required processor (OPN).
Refer below FAQ to read the device ID:
[FAQ] AM625/AM623 Custom board hardware design – Reading DEVICE_ID and Unique SOC (CPU) ID
The FAQ include information related to AM64x.
The recommendation is to update the processor OPN in the schematics with the chosen OPN.
For the list of available packages for AM64x and AM243x processor families, see the following FAQ:
For functional difference between ALV and ALX packages of AM243x processor family, see the following FAQ: