SPRAD67D September 2024 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The processor families support an integrated LDO (SDIO_LDO) to power the SDIO interface IO supply for IO group and SD card interface pullups, capable of dynamically switching between 3.3V and 1.8V voltage. The recommendation is to connect the recommended output capacitor close to the LDO output pin (CAP_VDDSHV_MMC1). For information on recommended, capacitor value and connection, refer to the Power Supply sub-section in the Signal Descriptions section of the device-specific data sheet.
V1P8_SIGNAL_ENA bit is used to switch the LDO output level used for controlling the SD card interface IO levels (signaling). The recommendation is to connect the supply connected to the SD card as input to SDIO_LDO. The output of the internal LDO can be connected to the processor IO supply for IO group used for SD card interface (VDDSHV5 for UHS-I SD card support).
For connecting the LDO pins (SDIO_LDO and CAP_VDDSHV_MMC1) when not used, see the Pin Connectivity Requirements section of the device-specific data sheet.
For more information, see the Integrated Low-dropout Regulator (LDO) section in the Power chapter of the device-specific TRM.