SPRU514Y August 2001 – June 2022
There are two user interfaces to the profiler mechanism. You can start and stop profiling in your application by using the following run-time-support calls.
This interface informs the run-time support that you wish to start profiling collection from this point on and causes the run-time support to clear all profiling counters in the application (that is, discard old counter values).
This interface directs the run-time support to stop profiling collection and output profiling data into the output file (into the default file or one specified by the TI_PROFDATA host environment variable). The run-time support also disables any further output of profile data into the output file during exit(), unless you call _TI_start_pprof_collection() again.