SPRUJ40F May   2022  – August 2026

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
  6. 2Hardware
    1. 2.1 System Description
      1. 2.1.1 Key Features
        1. 2.1.1.1 Thermal Compliance
        2. 2.1.1.2 Processor
        3. 2.1.1.3 Power Supply
        4. 2.1.1.4 Memory
        5. 2.1.1.5 JTAG/Emulator
        6. 2.1.1.6 Supported Interfaces and Peripherals
        7. 2.1.1.7 Expansion Connectors and Headers to Support Application Specific Add‐On Boards
      2. 2.1.2 Functional Block Diagram (SK-AM62 and SK-AM62B)
      3. 2.1.3 Functional Block Diagram (SK-AM62-P1 and SK-AM62B-P1)
      4. 2.1.4 AM62x SKEVM Interface Mapping
      5. 2.1.5 Power ON/OFF Procedures
        1. 2.1.5.1 Power-On Procedure
        2. 2.1.5.2 Power-Off Procedure
        3. 2.1.5.3 Power Test Points
        4. 2.1.5.4 Power Indication LED
      6. 2.1.6 Peripheral and Major Component Description
        1. 2.1.6.1  Clocking
          1. 2.1.6.1.1 Peripheral Reference Clock
        2. 2.1.6.2  Reset
        3. 2.1.6.3  OLDI Display Interface
        4. 2.1.6.4  CSI
        5. 2.1.6.5  Audio Codec Interface
        6. 2.1.6.6  HDMI Display Interface
        7. 2.1.6.7  JTAG Interface
        8. 2.1.6.8  Test Automation Header
        9. 2.1.6.9  UART Interface
        10. 2.1.6.10 USB Interface
          1. 2.1.6.10.1 USB 2.0 Type A Interface
          2. 2.1.6.10.2 USB 2.0 Type C Interface
        11. 2.1.6.11 Memory Interfaces
          1. 2.1.6.11.1 DDR4 Interface
          2. 2.1.6.11.2 OSPI
          3. 2.1.6.11.3 MMC Interfaces
            1. 2.1.6.11.3.1 MMC0 - eMMC Interface
            2. 2.1.6.11.3.2 MMC1 - Micro SD Interface
            3. 2.1.6.11.3.3 MMC2 - Wi-Fi Interface
          4. 2.1.6.11.4 EEPROM
        12. 2.1.6.12 Ethernet Interface
          1. 2.1.6.12.1 CPSW Ethernet PHY 2 Default Configuration
          2. 2.1.6.12.2 CPSW Ethernet PHY 1 Default Configuration
        13. 2.1.6.13 GPIO Port Expander
        14. 2.1.6.14 GPIO Mapping
        15. 2.1.6.15 Power
          1. 2.1.6.15.1 Power Requirements
          2. 2.1.6.15.2 Power Input
          3. 2.1.6.15.3 Power Supply
          4. 2.1.6.15.4 Power Sequencing
          5. 2.1.6.15.5 AM62x SoC Power
          6. 2.1.6.15.6 Current Monitoring
        16. 2.1.6.16 AM62x SKEVM User Setup and Configuration
          1. 2.1.6.16.1 EVM DIP Switches
          2. 2.1.6.16.2 Boot Modes
          3. 2.1.6.16.3 User Test LEDs
        17. 2.1.6.17 Expansion Headers
          1. 2.1.6.17.1 PRU Connector
          2. 2.1.6.17.2 User Expansion Connector
          3. 2.1.6.17.3 MCU Connector
        18. 2.1.6.18 Interrupt
        19. 2.1.6.19 I2C Address Mapping
  7. 3Additional Information
    1. 3.1 EVM Revisions and Assembly Variants
    2. 3.2 Known Issues and Modifications
      1. 3.2.1  Issue 1 - HDMI/DSS Incorrect Colors on E1
      2. 3.2.2  Issue 2 - J9 and J10 Header Alignment on E1
      3. 3.2.3  Issue 3 - USB Boot descoped on E1
      4. 3.2.4  Issue 4 - OLDI Connector Orientation and Pinout
      5. 3.2.5  Issue 5 - Bluetooth Descoped on E2 EVMs
      6. 3.2.6  Issue 6 - Ethernet PHY CLK Skew Default Strapping Changes
      7. 3.2.7  Issue 7 - TEST_POWERDOWN Changes
      8. 3.2.8  Issue 8 - MMC1_SDCD Spurious Interrupts
      9. 3.2.9  Issue 9 - PD Controller I2C2 IRQ Not Pinned Out
      10. 3.2.10 Issue 10 - INA Current Monitor Address Changes
      11. 3.2.11 Issue 11 - Test Automation I2C Buffer Changes
      12. 3.2.12 Issue 12 - ODLI Display Touch Broken
      13. 3.2.13 Issue 13 - Partial IO LPM Not Functional
    3. 3.3 Trademarks
    4.     87
  8. 4Compliance and Certifications
    1. 4.1 EMC, EMI and ESD Compliance
    2.     Regulatory Compliance
  9. 5References
  10. 6Revision History
Power Requirements

AM62x SKEVM can be powered through either of the two USB Type-C™ Connectors. Table 2-13 lists the descriptions of each connector.

Table 2-13 Connector Description
Connector Name Power Role Data Role
Connector 1 (J11) SINK None
Connector 2 (J13) DRP USB2.0 DFP or UFP

The AM62x SK EVM supports voltage input ranges from 5V to 15V and 3A of current. A USB PD controller (manufacturer part number: TPS65988DHRSHR) is used for PD negotiation upon cable detection to get necessary power required for the board. Connector 1 is configured to be an UFP port and has no data role. Connector 2 is configured as a DRP port, but connector 2 can only act as DFP when connector 2 powers the board. When both the connectors are connected to external power supply, the port with highest PD power contract powers the board.

Table 2-14 Type-C Port Power Roles
J11 (UFP) J13 (DRP) Board Power Remarks
Plugged in NC ON - J11 J11 becomes UFP and only sinks power and J13 can act as DFP if a peripheral is connected
NC Plugged in ON - J13 J13 becomes UFP and can only sink power
Plugged in Plugged in ON - J11 or J13 The port with highest PD power contract powers the board

The PD IC uses a SPI EEPROM to load the necessary configuration on power up to negotiate a power contract with a compatible power source.

The configuration file is loaded to the EEPROM using header J22. Once the EEPROM is programmed the PD obtains the configuration files via SPI communication. Upon loading the configuration files the PD negotiates with the source to obtain the necessary power requirement.

Note: The EEPROM is pre-programmed with the configuration file for the operation of the PD controller.

Power indication LEDs are provided for both the Type-C connectors for the user to identify which connector is powering the SKEVM Board.

An external power supply (Type-C output) can be used to power the EVM but is not included as part of the SKEVM kit.

The following are the external power supply requirements (Type-C):

  • Minimum Voltage: 5VDC, Recommended Minimum Current: 3000mA
  • Maximum Voltage: 15
  • VDC, Maximum current: 5000mA
Table 2-15 Recommended External Power Supply
DigiKey Part Number Manufacturer Manufacturer Part Number
1939-1794-ND GlobTek™, Inc. TR9CZ3000USBCG2R6BF2
Q1251-ND Qualtek™ QADC-65-20-08CB
Note: Because SK-AM62 implements USB PD for power, the device negotiates to the highest voltage and current combination supported by the device and power adapter. If the power adapter is compliant with the USB-C PD specification, the power supply can exceed the maximum voltage and current requirements listed above.