STDA041 October 2026 OPA690
In a voltage-to-current converter (V2I), the MOSFET must operate strictly in the saturation region to function as an ideal voltage-controlled current source. In saturation, the drain current ID is governed solely by VGS and is independent of VDS, giving the FET a high and well-defined trans-conductance gm. This makes sure that any step applied at the gate by the opamp is promptly and proportionally reflected at the source, allowing the feedback loop to settle quickly and accurately to the desired output current. However, if the FET is allowed to enter the ohmic (linear) region → where VDS < (VGS − Vth) → the device no longer behaves as a current source but instead transitions into a voltage-controlled resistor. In this region, the drain current becomes a function of both VGS and VDS, causing the effective trans-conductance gm to collapse significantly. As a result, when the opamp applies a step change at the gate, only a very small fraction of that step is replicated at the source — the gate-to-source signal transfer is severely attenuated. The feedback loop technically remains closed, but operating with a drastically reduced effective gain. This reduced effective gain forces the opamp to drive the gate harder and harder in an attempt to correct the error, yet each correction yields only a weak response from the FET. The loop continues to iterate through this low-gain corrective process, causing the output to settle very slowly before finally reaching the intended current level.