STDA041 October 2026 OPA690
The parasitic ESL of the sense resistor forms an L/R low-pass filter with Rsense, since the feedback voltage VFB is sensed directly across Rsense. During a current transient, the ESL opposes the rapid change in current, and the feedback voltage only settles to the true value after a time-constant of τ = ESL+ LSource / Rsense, giving a rise-time of approximately:
This creates a fundamental conflict, reducing Rsense minimizes power dissipation but directly increases the L/R time constant and slows down the feedback response, resulting in a rise-time beyond the required specification. Therefore, Rsense cannot be reduced arbitrarily, and the rise-time constraint sets a lower limit for Rsense.