SWAU132A April   2024  – August 2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Regulatory Compliance
      1. 1.3.1 Waste Electrical and Electronic Equipment (WEEE)
    4. 1.4 Specification
    5. 1.5 Device Information
  6. 2Hardware
    1. 2.1 Hardware Features
    2. 2.2 Connector and Jumper Descriptions
      1. 2.2.1 LED Indicators
      2. 2.2.2 Jumper Settings
      3. 2.2.3 BoosterPack Header Assignment
      4. 2.2.4 JTAG Headers
    3. 2.3 Power
      1. 2.3.1 Measure the CC3351 Current Draw
        1. 2.3.1.1 Low Current Measurement (LPDS)
        2. 2.3.1.2 Active Current Measurement
    4. 2.4 Clocking
    5. 2.5 Performing Conducted Testing
  7. 3Implementation Results
    1. 3.1 Evaluation Setups
      1. 3.1.1 MCU and RTOS
      2. 3.1.2 Processor and Linux
      3. 3.1.3 Standalone RF Testing
        1. 3.1.3.1 Radio Tool BP-CC3351 Hardware Setup
  8. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  9. 5Additional Information
    1. 5.1 Support Resources
    2. 5.2 Trademarks
  10. 6Revision History

Processor and Linux

The BP-CC3351 can integrate with a host platform running Linux OS, like the BeagleBoard.org® BeagleBone® Black (BBB). The BeagleBone Black is a low-cost, community-supported development platform as shown below.

BP-CC3351 BeagleBone Black BoardFigure 3-2 BeagleBone Black Board

To interface with the BP-CC3351 with the BeagleBone Black, the user also needs the BP-CC33-BBB-ADAPT to BBB Adapter Board .

BP-CC3351 Adapter Board for the BeagleBone BlackFigure 3-3 Adapter Board for the BeagleBone Black
BP-CC3351 BP-CC3351 and BBB with Adapter BoardFigure 3-4 BP-CC3351 and BBB with Adapter Board

To make sure the BeagleBone Black boots up from the SD card, TI recommends to a remove the 100kohm resistor R68 seen on the bottom of the BBB, and add as R93 on the top of the BBB. Alternatively, press and hold the S2 button on the BeagleBone board during power-up if the hardware modifications were not made. (See Figure 3-5 and Figure 3-6.)

Lastly, adding a right-angle header on the bottom of the BBB to easily connect the FTDI cable is optional. When the adapter board is attached to the BBB, the FTDI cable can get pinched between the BBB and the adapter board, which can cause communication problems. (See Figure 3-6.)

BP-CC3351 Modified BBB (Bottom
                    View) Figure 3-5 Modified BBB (Bottom View)
BP-CC3351 Modified BBB (Top View)Figure 3-6 Modified BBB (Top View)