SWRA370A September   2011  – December 2025 CC1100 , CC1101 , CC2340R5-Q1 , CC2500 , CC2510 , CC2520 , CC2530 , CC2530-RF4CE , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F-Q1 , CC2642R-Q1 , CC2662R-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Acronyms
  5. 2Standards and System Requirements
    1. 2.1 Standards
    2. 2.2 Test Equipment Suppliers
    3. 2.3 Radio Certification URLs
  6. 3Test Equipment Requirements
    1. 3.1 System Setup
      1. 3.1.1 Conducted Test Systems
      2. 3.1.2 Radiated Test Systems
    2. 3.2 Initial Considerations for Testing
    3. 3.3 Testing Reminders
  7. 4Software Setup
    1. 4.1 SmartRF Studio 7
      1. 4.1.1 SmartRF Studio 7 Start-Up Window
      2. 4.1.2 SmartRF Studio 7 Modes
      3. 4.1.3 SmartRF Studio 7 Device Control Panel
      4. 4.1.4 SmartRF Studio 7 Software User Manual
    2. 4.2 SmartRF Studio 8
      1. 4.2.1 SmartRF Studio 8 Start-Up Window
      2. 4.2.2 SmartRF Studio 8 Radio Control Window
      3. 4.2.3 SmartRF Studio 8 Software User Guide
  8. 5DUT and Test Instrument Information
    1. 5.1 DUT
    2. 5.2 Test Instruments
  9. 6Clock Frequency Tuning
    1. 6.1 HF Clock Tuning Utilizing the Internal Cap Array
    2. 6.2 LF Clock Tuning
  10. 7Transmission Tests
    1. 7.1 Transmission Power
    2. 7.2 Power Spectral Density Mask
    3. 7.3 Error Vector Magnitude
    4. 7.4 Transmission Center Frequency Offset
    5. 7.5 Spurious Emissions
  11. 8Receive Testing
    1. 8.1 Receiver Sensitivity
    2. 8.2 Interference Testing
    3. 8.3 Interference Testing with RF Generator
  12.   Appendix A Offset EVM vs. EVM
  13.   B References
  14.   B Revision History

Interference Testing

Purpose: To verify that the receiver sensitivity conforms to the published standards.

Pass Condition: See respective standards document for specifications and pass conditions.

Test Environment: Figure 8-5 illustrates the interference test setup.

 Interference Testing Setup Diagram Figure 8-5 Interference Testing Setup Diagram
 Interference Testing Bench Setup - Overview Figure 8-6 Interference Testing Bench Setup - Overview
 Interference Testing Bench Setup - Shielded Box Figure 8-7 Interference Testing Bench Setup - Shielded Box
 Interference Testing Bench Setup - TX and interferer connections Figure 8-8 Interference Testing Bench Setup - TX and interferer connections
Note: If there is no variable attenuator available, a series of fixed attenuators can be used instead. Also, a combination of variable and fixed attenuators can be used to increase the attenuation factor, as depicted in Figure 8-8. Figure 8-8.

Procedure:

  • Step 1: Connect the instruments as shown on Figure 8-5, Figure 8-6, Figure 8-7, and Figure 8-8.
  • Step 2: Use the same configuration from the sensitivity test 8.1, for the TX and RX boards.
  • Step 3: Setup the INT (interference) board as a transmitter; however, the frequency can be different than that of either the TX and RX signals. If testing for co-channel interference, the frequency should be the same, otherwise, frequency should vary. Furthermore, unlike the TX that transmits packets, the INT transmits continuously (that is, it is a continuous modulated signal).
  • Step 4: Set the output power of the TX such that the received power at the RX end is 10dB above the sensitivity threshold obtained from sensitivity testing. This is also dependent on the standard. (Remove 10dB of attenuation from the attenuators after completing the sensitivity test.)
  • Step 5: Initially, set the output power of the INT board to the lowesr output power setting possible and start transmitting.
  • Step 6: Perform the sensitivity test between the RX and TX board and notate the PER. Continue to increase the output power of the INT until the PER, displayed on the RX side, is greater than 1%. The difference between the TX and INT power measured on the RX side indicates the ability of the CCxxxx device to overcome interference.
Table 8-3 Adjacent Channel Test Results
Channel Frequency (MHz) Difference (dB) Design Specification (dB) Pass/Fail?
1
2
3
Table 8-4 Alternate Channel Test Results
Channel Frequency (MHz) Difference (dB) Design Specification (dB) Pass/Fail?
1
2
3
Test Results: