SWRA370A September 2011 – December 2025 CC1100 , CC1101 , CC2340R5-Q1 , CC2500 , CC2510 , CC2520 , CC2530 , CC2530-RF4CE , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F-Q1 , CC2642R-Q1 , CC2662R-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1
Purpose: Transmission modulation accuracy is measured using error vector magnitude (EVM). EVM, as illustrated in Figure 7-8 and Figure 7-9, is the magnitude of the phase difference as a function of time between an ideal reference signal and the measured transmitted signal.
Figure 7-8 Error
Vector Magnitude
Figure 7-9 EVM and
Related QuantitiesPass Condition: See the respective standards document for specifications and pass conditions.
Test Environment: Figure 7-10 illustrates the setup for the EVM test. Figure 7-10
Figure 7-10 Error
Vector Magnitude Test Setup Diagram
Figure 7-11 Error
Vector Magnitude Test Bench Setup Using An SMA Connector
Figure 7-12 Error
Vector Magnitude Test Bench Setup Using An AntennaProcedure:
Example: EVM measurements on ZigBee signals using a Rohde & Schwarz FSQ can be set up following the instructions in Ref. 1.
Note that not all spectrum analyzers will work on this test, they must have the capability and be configured to do EVM measurements to do so.| EVM (%) at ____ kbp/s | Design Specification (%) | Pass/Fail? | |||
|---|---|---|---|---|---|
| Freq 1 (MHz) | Freq 2 (MHz) | Freq 3 (MHz) | |||
| 1 | |||||
| 2 | |||||