SWRA825 January 2025 IWR6843 , LP87745-Q1
Two radar sensors are placed in the same physical location, creating overlapping fields of view. It reduces the installation cost since both sensors are mounted together. But the hardware costs are still higher compared to mono-static configurations.
Figure 3-8 Co-Located Bi-Static Setup
(Two Sensor Products)Environmental factors with a coupling effect, such as mechanical vibrations in the supporting structure add new dependent fault injectors (DFI). A mitigation strategy could be to use signal-to-noise ratio (SNR) measurements or onboard vibration sensors to detect and manage faults caused by vibrations.