SWRZ101C December 2021 – May 2025 AM2732 , AM2732-Q1
MibSPI: MibSPI RX RAM RXEMPTY Bit Does Not Get Cleared After Reading
The RXEMPTY flag may not be auto-cleared after a CPU or DMA read when the following conditions are met:
If at all possible, avoid transfer groups interrupting one another. If dummy buffers are used in lower-priority transfer groups, select the appropriate "BUFMODE" for them (like, SKIP/DISABLED) unless, there is a specific need to use the "SUSPEND" mode.