TIDUF26 june 2023 BQ24072 , LMR36520 , TLV62568 , TPS2116
TIDA-010932 also integrates an INA2180 (Figure 2-11) for current sensing of the two power rails (5 V from LMR36520 and 5 V from USB). The output of this device is also tied to the BoosterPack™ header for easier data collection as well as the ability to monitor system power if an MCU LaunchPad™ is connected.
Figure 2-11 INA2180 Power Rail Current
Sensing CircuitThe accuracy of the INAx180 is maximized by choosing the current-sense resistor to be as large as possible. A large sense resistor maximizes the differential input signal for a given amount of current flow and reduces the error contribution of the offset voltage. However, there are practical limits as to how large the current-sense resistor can be in a given application. Equation 19 gives the maximum value for the current sense resistor for a given power dissipation budget:
where
To make sure that the current-sense signal is properly passed to the output, both positive and negative output swing limitations must be examined. Equation 20 provides the maximum values of RSENSE and GAIN to keep the device from hitting the positive swing limitation.
where
The negative swing limitation places a limit on how small of a sense resistor can be used in a given application. Equation 21 provides the limit on the minimum size of the sense resistor.
where