TIDUF72 August 2024
Utility providers and customers are driving the need for more features from electricity meters. As the accuracy requirements and amount of processing expected from electricity meters rapidly increase, it becomes more and more difficult to solve these issues with a single metrology system-on-chip (SoC). A dual-chip approach with a standalone ADC and a host microcontroller (MCU) helps overcome the limitations of electricity meter SoCs and enables a mix-and-match solution, which can be optimized for cost or performance.
Using an accurate state-of-the-art standalone ADC with integrated power and data isolation, such as the AMC131M03, has the following advantages:
To properly measure energy consumption, voltage, and current sensors, translate mains voltage and current to a voltage range that an ADC can detect. When a multiphase power distribution system is used, it is necessary for the current sensors to be isolated from phase-to-phase, so the sensors can properly detect the current drawn from one or two different lines (when neutral is measured or in split-phase configuration) without damaging the ADCs. This design uses two cost-effective shunt sensors, which are immune to magnetic tampering, and enables the implementation of electricity meters for single-phase with optional neutral line measurement or split-phase meters with two currents and a single voltage configuration.
TIDA-010944 is a class 0.2 S high-accuracy one-phase or split-phase SHUNT electricity meter reference design, using one three-channel standalone isolated AMC131M03 ADC, one non-isolated two-channel standalone ADS131M02 ADC, and a cost-effective MSPM0G1106 MCU. The reference design can also be used for energy metering in popular products such as electric vehicle (EV) chargers and AC wall boxes. The non-isolated ADCs senses the current and the voltage on Phase A, while the non-isolated ADC is used for current monitoring of the Neutral line or Phase B, depending on which configuration is used.
The TIDA-010944 firmware specifically supports calculation of various metrology parameters for single-phase with Neutral line or split-phase energy measurement. These parameters can be viewed from the calibration GUI or through the ACT and REACT pulsed outputs, connected to a reference metrology test system.