For this design, follow these general
guidelines:
- Place decoupling capacitors close to the associated pins.
- Use ground planes instead of ground traces and
minimize the cuts in the ground plane, especially near the ADS131M02 and
AMC131M03. In this design, there is a ground plane on both the top and bottom
layer for the HGND (high voltage side) for both Phase A and Phase B. Make sure
that there is good stitching between the planes through the liberal use of
vias.
- Keep the two traces to the inputs of each ADC channel symmetrical and as close as possible to each other.
- Crosstalk from the voltage to current channels can reduce accuracy at lower currents if power offset is not performed.
- For the ADS131M02 and AMC131M03 devices, place
the 0.1μF capacitor closer to the AVDD pin than the 1μF capacitor. Do the same
thing for the 0.1μF and 1μF capacitors connected to DVDD.
- Minimize the length of the traces used to connect
the crystal to the microcontroller. Place guard rings around the leads of the
crystal and ground the crystal housing. In addition, there must be clean ground
underneath the crystal and avoid placing any traces underneath the crystal.
Also, keep high-frequency signals away from the crystal.
- Use wide traces for power-supply connections.
- Use a different ground plane for the isolated RS-232. This other ground plane is at the potential of the RS-232 ground and not the GND used elsewhere in the board.
- Make sure that the recommended clearance and creepage spacing are met for the ISO6731 isolation device.