TIDUF72 August 2024
Figure 2-5 shows that the analog front end for current inputs is different from the analog front end for the voltage inputs.
Figure 2-5 Analog Front End for Current
InputThe positive and negative leads from the SHUNT sensor are connected to pins 1 and 2 of header J14 (for Phase A). The analog front end for current consists of footprints for electromagnetic interference filter beads (FB5 and FB6), and a two-stage RC low-pass filter (R74, R81, C30, C34) and R34, R35, and C38 that functions as an anti-aliasing filter.
Equation 2 shows how to calculate the range of differential voltages fed to the current ADC channel for a given maximum current, and shunt resistor value.

Assuming a SHUNT value of 150μΩ, the input signal to the current ADC has a voltage swing of ±21,21mV when the maximum current rating of the meter (100A) is applied. This relatively low voltage, when using GAIN = 32 is well within the required Full-Scale Range of ±37.5mV. See also full-scale range table in the AMC131M03 3-Channel, 64-kSPS, Simultaneous-Sampling, 24-Bit, Reinforced Isolated Delta-Sigma ADC With Integrated DC/DC Converter data sheet.