Low-noise low-dropout regulators (LDO) are
required in many applications to make sure that power supply noise
does not couple into the signal chain. The requirements for LDO
output current continue to increase as new sensors require
additional current or different loads are combined to save space.
Using a single LDO for the supply is not always possible due to
power dissipation limitations or output current capability. The
TIDA-050096 reference design solves this issue by using multiple
LDOs configured to share current in parallel. There are two methods
for paralleling the TPS7B7702-Q1 in this reference design:
- Operational Amplifiers: The first method
uses op amps to parallel multiple TPS7B7702-Q1
channels. A wide range of op amps can be used to
parallel the TPS7B7702-Q1, including the OPA388-Q1
and LMV321A-Q1. Up to four TPS7B7702-Q1 channels are
paralleled in this reference design, using op amps,
to deliver up to 1.2A to the load while maintaining
all of the key features of a single TPS7B7702-Q1
channel. This approach can be scaled above four LDO
channels; however, there is no limit to the number
of channels that can be placed in parallel using
this technique.
- Ballast Resistors: The second method uses
ballast resistors, which can be designed either as
discrete resistors or as copper traces on the
printed-circuit board (PCB). In some applications,
the harness resistance inherent in the system can
also be used as part as all of the ballast
resistance. Although there is no theoretical limit
to the number of TPS7B7702-Q1 LDO channels that can
be paralleled using this technique, Texas
Instruments recommends limiting the number to two
channels. This is recommended because the error
voltage, or difference between the output of each
individual LDO[1], increases with output voltage as a
result of the gain set by the feedback resistors. At
higher voltages, the increased gain amplifies the
error voltage, leading to larger ballast resistance
values - potentially exceeding 1Ω for the
TPS7B7702-Q1. Increasing ballast resistance can
lead to an impractical approach given the adverse
impact on load regulation.