JAJSSJ5 December 2023 DRV8234
PRODUCTION DATA
Denoted by INV_R_SCALE, this is the scaling factor for the inverse of motor resistance (INV_R). Since the inverse of a motor resistance is generally not an integer, the value must be rounded off to the nearest integer. Settings are described in Section 7.3.6.1.2.
Bit | Value of INV_R_SCALE |
---|---|
00b | 2 |
01b | 64 |
10b | 1024 |
11b | 8192 |
INV_R is represented by the equation:
Please note that the maximum value of INV_R is 255.