JAJSCG5C July 2016 – June 2018 TPS546C23
PRODUCTION DATA.
This bit selects between two options for low-side FET behavior after an output overvoltage fault condition. Regardless of the setting of this bit, the low-side FET latches on when an output OV fault is detected (if the OV_FAULT_RESPONSE is not programmed to ignore).
BIT VALUE | ACTION |
---|---|
0 | The low-side FET remains on until either the part initiates a new startup of the output voltage or the CLEAR_FAULTS command is given while the part is in the DISABLE operational state |
1 | The low-side FET turns off as soon as the sensed output (at FB pin) drops below 0.2 V. |